ARM Processor Dev Kits
ARM MCU Dev Kits
element14
DESIGN CENTER BETA
Find the latest development tools and kits in one place! Visit element14 Design Center today!
Learn MorePlease select the type of assistance you require
We will no longer be supporting Internet Explorer, to ensure you have the best possible experience we recommend using a modern browser.
Order Code
Manufacturer
Quantity
Pack Size
Unit Price (excl GST)
Re-reeling Charge
Order Code
Manufacturer
Quantity
Unit Price (excl GST)
items have been added to your basket
Review your cart for details on availability and shipping
Your Basket is Empty
| Description | Order Code | Manufacturer | Quantity | Total (excl GST) |
|---|
Please note: you already have a quotation in your basket related to another account. You may only checkout a basket for a single account at any one time. Should you require a new quote for a different account please contact our sales team on [INSERT TEL OR EMAIL]
You have a quotation in your basket related to a different account than the items you are now trying to add.Please complete the purchase (or remove the quote – don't worry it's still available in My Account) before adding these additional items.If you continue, your current basket will be overwritten.
Your quotation can only be purchased against the specific associated billing account.Items in your basket are related to a different account. Please save the current basket or complete the purchase before adding these additional quote items.If you continue, your current basket will be overwritten.
Our ever-expanding range of solutions offers everything you need at any stage of your design - from starter kits to complete development boards and tools, including the newest releases for Embedded, Analog, Sensing and Wireless from leading manufacturers such as Analog Devices, Atmel, Microchip, NXP, STMicroelectronics, Texas Instruments and more.
An open source evaluation platform featuring the powerful i.MX 6Solo, a multimedia application processor with ARM® Cortex-A9 core at 1 GHz to evaluate the rich set of peripherals which includes 10/100/Gb Ethernet port, HDMI v1.4, LVDS and more.
Ultra-low-cost development platform featuring the Kinetis series of microcontrollers (which are based on ARM® Cortex-M0+ and Cortex-M4 cores) in a conveniently small form factor.
A low-cost development platform based on NXP's I.MX 6Quad ARM® Cortex-A9 application processor which enables users to quickly start their development and support Linux 3.0.15 or Android 4.0.4.
A low cost fully featured, internet enabled development platform based on Sitara™ AM3358 ARM® Cortex™-A8 processor from Texas Instruments that runs on a variety of OS including Debian, Angstrom, Ubuntu & Android, together with the wide array of accessory boards to address the needs of designers, early adopters, and anyone in the Open Source Community.
A low cost highly integrated controller board based on NXP's i.MX 6 Dual ARM® Cortex-A9 application processor which encompasses a dual core platform running up to 1GHz with 1MB of L2 cache and 64bit DDR3 or 2-ch, 32bit LPDDR2 support.
A full featured FPGA evaluation board which harnesses the power of a Cyclone V SoC from Altera.
A single board computer based on Texas Instruments DM3730 DaVinci digital media processor with 4.3inch LCD.
Platform for smart devices based on i.MX 6 Quad processor, the latest in a series of high performance, highly integrated development kits targeted for any application that require an intelligent display, connectivity, low power consumption, an amazing user experience and broad operating system support that includes Android, Linux and Windows Embedded.
An easy-to-use and inexpensive development platform that gives designers the power of an ARM® Cortex-M0 combined with the fully customizable analog and digital fabric of the PSoC, enabling the designers to create unique designs with the flexibility of PSoC 4.
Includes everything required for beginners and experienced users to get started. Quickly discover the STM32F4's high-performance features and develop user applications easily.
Comprises a target board combined with a JTAG debugger and designed to make it as easy as possible to get started with Cortex-M0.
Industry's first single-chip programmable microcontroller with built-in Wi-Fi connectivity, the SimpleLink™ CC3200 device is a wireless MCU that integrates a high-performance ARM® Cortex-M4 MCU for developing an entire application with a single IC.
A fast prototyping & low cost evaluation platform based on the SAMA5D3 Atmel’s ARM® Cortex®-A5 processor-based MPU and come pre-loaded with a Linux-based embedded operating system for industrial, wearable computing and mobile applications.
Mounted with ARM® Cortex™-M0 based XMC1100 Microcontroller with two rows of pin headers which are fully compatible with Arduino™ shield. Users can buy various Arduino shield boards off-the-shelf to test the capabilities of XMC1100 Microcontroller.
Find the latest development tools and kits in one place! Visit element14 Design Center today!
Learn More