ROBOTICS

Automatic Guided Vehicle - AGV

Automatic Guided Vehicle (AGV) is a type of unmanned wheel-driven robot. Under the instructions given by monitoring system, it is able to find the specified destination through predetermined route by utilizing automatic guide devices and on-board sensors and then complete assigned tasks. Due to advantages of agility and intelligence, AGV is mainly used in applications such as flexible manufacturing systems and smart warehouses.

More

An AGV device is composed of a variety of modules for navigation, movement, obstacle detection, loading/unloading, communication and power supply. Navigation is certainly the key function. Nowadays, navigation methods adopted in AGV include electromagnetic, magnetic stripe, optical, infrared, laser and visual navigation. Laser navigation is a popular method used in AGV due to its high agility and accurate control. To implement laser navigation, a great number of rectangular prisms that can reflect laser back to vehicles are required to be fixed on walls and obstacles, and laser transceivers that can rotate horizontally should be mounted on top of vehicles. When vehicles are moving, the real-time location can be calculated based on incident angle and prisms’ positions, and then compared with the predetermined route stored in memory to accurately adjust vehicles’ movement.

The movement module of an AGV is made up of motors, motor control units and driving circuits. Vehicles’ speed is controlled by processor. The moving direction of vehicles changes when the motors on both sides are rotating at different speed. During movement, AGV needs an ultrasonic or infrared sensor to detect obstacles standing in its way. Furthermore, an accelerometer is used to detect the inclination of ground in order to prevent fall of loaded goods. AGV’s loading/unloading module is used to load and unload goods by driving a motor to control forklift. Battery is used as power supply of AGV. When low power is detected, monitoring system gives vehicles an instruction to go to a specific position to charge automatically.

With the development of sensor technology, multiple navigation and obstacle detection methods could be combined together to realize AGVs with more intelligence and accuracy.

Less

Hover over the diagram blocks to view recommended products for this solution:

Used for processing signals from sensors, calculating AGV's location in real time as well as ensuring that the AGV moves along specified route.
Click for full parts list

Used for processing signals from sensors, calculating AGV's location in real time as well as ensuring that the AGV moves along specified route.
Click for full parts list

Drives stepper motor to rotate laser transceiver horizontally.
Click for full parts list

A low-voltage, high-current gate driver should be used to drive MOSFET.
Click for full parts list

Used for driving high-power motor so that AGV can move and perform loading/unloading.
Click for full parts list

Used for driving high-power motor so that AGV can move and perform loading/unloading.
Click for full parts list

Laser Transmitter.
Click for full parts list

Laser transceiver to receive laser reflected from rectangular prisms.
Click for full parts list

Infrared sensor is used to detect obstacles in short distance.
Click for full parts list

Ultrasonic sensor is used to detect obstacles in short distance.
Click for full parts list

Three-axis accelerometer detects inclination of ground during movement of AGV.
Click for full parts list

It monitors the motor's rotational parameters.
Click for full parts list

It monitors the motor's rotational parameters.
Click for full parts list