This promotion ends on 15th May 2019. Limited FREE GIFTS available, get them while it lasts!
 Order ValuePromotion CodeGiftImage
1Order value > $100PROMO2BWeather Resistant Cable Ties Pack of 100Cable Tie Pack of 100
2Order value > $100PROMO2DPlier Set, Snap Ring, Circlip, 180°/90°/45° x 3Plier Set
3Order value > $100PROMO3ATrolley, Dolly, Plastic, 100kg Max LoadTrolley
4Order value > $100PROMO3BSoldering Tip CleanerSolder Tip Cleaner
5Order value > $100PROMO3CTorch, with Head Strap, 3W, Head Light, LED, 160LM, 100mHead Torch
6Order value > $100Solder Iron
7Order value > $100PROMO4CBreadboard, Solderless, ABSBreadboard
8Order value > $100PROMO5ABattery, Ultra, Pack of 40, 1.5 V, AAA, AlkalineBatteries
9Order value > $150Multimeter
10Order value > $150PROMO5CScrewdriver Set, Insulated, 8 PiecesMultimeter
11Order value > $150Multimeter
12Order value > $250PROMO5EPickup Tool Set, Vacuum, 132 mm LengthSolder Wire
13Order value > $250PROMO6BGlue Gun, 60W, 230VGlue Gun
14Order value > $250ECARD20AUGift card (Coles & Myer Gift card)

Gift card (Coles & Myer Gift card)

15Order value > $500PROMO6CFume Extractor, ESD, Bench MountFume Extractor
16Order value > $500PROMO6DRpi 3 - Raspberry Pi 3 B+Raspeberry Pi 3B+
17Order value > $500PROMO6EDigital Multimeter, 6000 Count, True RMSMultimeter
While stocks last
HAKKO - Soldering Station, Digital, 70 W, 450 °C

HAKKO - Soldering Station, Digital, 70 W, 450 °C

Was: $683.11 Now: $614.79

Buy now
While stocks last
HAKKO - Soldering Station, Digital, 70 W, 480 °C

HAKKO - Soldering Station, Digital, 70 W, 480 °C

Was: $248.00 Now: $197.00

Buy now
Hot!
HAKKO - Soldering Station, Analogue, 75 W, 450 °C Max Temperature

HAKKO - Soldering Station, Analogue, 75 W, 450 °C Max Temperature

Was: $636.70 Now: $541.20

Buy now
Stock up now while it lasts

*Prices shown on website already have discounts.

25% Off
Pocket Digital Multimeter

Pocket Digital Multimeter

Was: $48.04 Now: $34.31

Buy now
25% Off
Professional Digital Multimeter

Professional Digital Multimeter

Was: $113.68 Now: $85.26

Buy now
25% Off
Digital Multimeter

Digital Multimeter

Was: $434.44 Now: $310.31

Buy now
25% Off
Handheld Digital Multimeter

Handheld Digital Multimeter

Was: $71.91 Now: $52.73

Buy now
25% Off
Handheld Digital Multimeter

Handheld Digital Multimeter

Was: $107.91 Now: $79.13

Buy now
Stock up now while it lasts

*Prices shown on website already have discounts.

1

Separately: $136.26 Bundle: $100.47

2

Separately: $102.82 Bundle: $78.97

3

Separately: $433.60 Bundle: $368.52

5% Off
3D Printer, 1.75 mm Filament, 180 mm/s Speed, 200 mm x 200 mm x 200 mm Build

3D Printer, 1.75 mm Filament, 180 mm/s Speed, 200 mm x 200 mm x 200 mm Build

Was: $1237.10 Now: $1175.25

Buy now

Save 25% on Multicomp 3D Printer Filament

DescriptionWasNow#
3D Printer Filament, 1.75 mm, PLA, Black, 1 kg$30.65$22.99Buy now
3D Printer Filament, 1.75 mm, PLA, Blue, 1 kg$30.65$22.99Buy now
3D Printer Filament, 1.75 mm, PLA, Brown, 1 kg$30.65$22.99Buy now
3D Printer Filament, 1.75 mm, PLA, Gold, 1 kg$30.65$22.99Buy now
3D Printer Filament, 1.75 mm, PLA, Green, 1 kg$30.65$22.99Buy now
3D Printer Filament, 1.75 mm, PLA, Grey, 1 kg$30.65$22.99Buy now
3D Printer Filament, 1.75 mm, PLA, Orange, 1 kg$30.65$22.99Buy now
3D Printer Filament, 1.75 mm, PLA, Red, 1 kg$30.65$22.99Buy now
3D Printer Filament, 1.75 mm, PLA, Silver, 1 kg$30.65$22.99Buy now
3D Printer Filament, 1.75 mm, PLA, White, 1 kg$30.65$22.99Buy now
3D Printer Filament, 1.75 mm, PLA, Yellow, 1 kg$30.65$22.99Buy now

How to redeem free gift:

  1. Add products to basket
  2. Click on 'Shopping Basket' Tab
  3. Click on 'Checkout Securely'
  4. Select 'Others' from the 'Special Instructions' drop down menu and input respective promotion code
  5. Confirm order

Terms & conditions for the free gift

  1. Web orders only.
  2. The free gift promotion is valid until 15th May 2019, or while stocks last, whichever is the earliest.
  3. Customers must quote or enter the valid promo code at the checkout when ordering or when they call or email their order.
  4. Promo codes cannot be added to any order after the order has already been submitted.
  5. Promo code can be used on next order while the promotion is still on-going.
  6. If the Free gift card is chosen, please note that the gift card will be posted after the promotion, on or before 22nd May 2019.
  7. If purchasing online please add the Promo code on below instructions:
    • Choose "Other" from the "Special Instructions" drop down menu and type the corresponding promo code
    • Click on "Confirm Order" button.
  8. The required minimum value does not include freight, GST or discounts and must be placed in one transaction.
  9. The free gifts promo codes are not available in conjunction with any other discounts or offers.
  10. This offer is not available for customers who are already receiving special pricing.
  11. Changes may be made to products by our suppliers, the images shown are for reference only.
  12. element14 reserves the sole discretion on deciding whether a sale qualifies for the program and has the right to cancel or modify the promotion at any time without prior notification.